| Solutions | Lighting technology | LED | Overview | Solutions | Lighting technology | LED | Overview

LED

LED

  • 2060 Series
    2060 Series
  • 250 Series
    250 Series
  • 744 Series
    744 Series
  • 804 Series
    804 Series
  • 805 Series
    805 Series

"Efficiency" is the buzzword of the LEDs. The electronic semiconductors convert about 90% of the electrical energy into light waves. By comparison, light bulbs just about 10%. LEDs are insensitive to vibration and shock and give off little heat and no UV radiation. LED technology opens up new possibilities for designing LED lights.SMD Terminal Blocks, 2060 Series. Here, the connection method must not only follow the requirements of the design and functionality, but also provide an operating concept that is already familiar to the user. This requires a vision in the development of the connection technology. With the SMD PCB terminals Series 2060 WAGO offers a solution for SMD applications or applications that require several connections in a small space.

For plug-in applications, there are numerous options due to the WAGO MCS(and) WINSTA®Program For LED drivers that are exposed to rough environmental conditions, WAGO has developed the heavy-duty terminals of Series 804 (and) 805 For more conventional designs you will find the Series 250 (and) 744 useful.
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
../../../../navigation-complete.html